Industry Online Support
Technical Forum
7/31/2006 12:01 PM | |
Posts: 3149 Rating: (171)
|
Hi, first of all, please install SP4 for WinCC v6.0 and then check the diagnose files in the folder ..\wincc\diagnose for entries/erros. nemo |
7/31/2006 12:16 PM | |
Posts: 68 Rating: (0) |
Thanks Nemo, Can I download the SP4 from anywhere ? |
7/31/2006 12:26 PM | |
Posts: 3149 Rating: (171)
|
Hi here you can download, please check the compatiblity before installing SP4: SP4 for WinCC V6.0. http://support.automation.siemens.com/WW/view/en/22303359 and check the compatibility with your operating system: http://support.automation.siemens.com/WW/view/en/21927773 nemo |
8/3/2006 10:32 AM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating: (151)
|
Be careful. Upgrading WinCC means you also need to upgrade any options/software used, such as WebNavigator, Simatic NET, Step7. Details are in the FAQ Nemo posted above. You do not mention which Global Script Editor you are using, C or VBS. If it is the VBS Editor then installing Hotfix 2 for SP3 will probably resolve the problem. European - http://support.automation.siemens.com/WW/view/en/21480479 Asian - http://support.automation.siemens.com/WW/view/en/22128061 |
Follow us on