8/8/2017 12:13 PM | |
Joined: 4/4/2015 Last visit: 12/4/2020 Posts: 12 Rating:
|
Dear All I have a problem getting connecting using 2 S7-1200 PLC with GPRS Module. I am using SIM cards with Fixed IP Addresses in both PLC. Reading manual it says it should be with Port 30000, but i cant find how to change port, also i dont know if i make right configuration specifically on TCON_IP_RFC block. In online mode the TCON instruction give status "7002". Please can anyone help. Thanks in advance AttachmentS7-1200.docx (48 Downloads) |
Follow us on