7/7/2017 10:09 AM | |
Posts: 648 Rating: (95) |
Dear djpiky_1, in the PLC you can define alarms for:
This example could be helpful to define your own PLC alarms https://support.industry.siemens.com/cs/ww/en/view/98210758 If you use more than two standard alarm classes (No Ack and Ack) you have to define your own classes. Open in the project navigation "Common data > alarms classes" and create your own classes. In the HMI you can read the alarms from the plcs. Open "HMI alarms > PLC alarms" and get all defind alarms To show the alarms in the HMI use the alarm control. Open the properties of the control. Under "General > Display > Current Alarm states" you can define, which classes should be shown. With best regards rh1990
|
Follow us on