10/11/2018 2:59 PM | |
Joined: 10/17/2011 Last visit: 7/19/2022 Posts: 148 Rating: (3) |
Hi, I need gsdml file for 6ES7 155-6AU00-0CN0 having firmware version 3.3. Thanks, Damayanti ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 10/12/2018 9:08:22 AMNew subject after splitting |
|
10/11/2018 5:12 PM | |
Joined: 9/27/2006 Last visit: 11/14/2024 Posts: 12294 Rating: (2691) |
Hello Damayanti; This dlownload contains the current version of the gsdml file for your ET 200SP.. Note that your part number is inserted in the Associated Products tab. https://support.industry.siemens.com/cs/ww/en/view/57138621 If for some reason it does not fit your requirements, you must contact Product Support (using the Support Request link at the top of this page) and ask for more help from Siemens techs. Hope this helps, Daniel Chartier |
10/12/2018 10:08 PM | |
Joined: 9/27/2006 Last visit: 11/14/2024 Posts: 12294 Rating: (2691) |
Hello Damayanti; What will be your CPU, and what optional Safety software do you plan to use? See for example this manual for Safety Basic/Advanced v15: SIMATIC Industrial Software SIMATIC Safety - Configuring and Programming https://support.industry.siemens.com/cs/ww/en/view/54110126 STEP 7 Safety optional packages This documentation describes the optional packages STEP 7 Safety Advanced V15 and STEP 7 Safety Basic V15. The STEP 7 Safety optional packages are the configuration and programming software for the SIMATIC Safety F-system. With STEP 7 Safety, you receive the following: ● Support for configuring the F-I/O in the hardware and network editor of the TIA Portal ● Support for creating the safety program using LAD and FBD and integrating error detection functions into the safety program ● Instructions for programming your safety program in LAD and FBD, which you are familiar with from the standard user programs ● Instructions for programming your safety program in LAD and FBD with special safety functions Moreover, STEP 7 Safety offers functions for comparing safety programs and for assisting you with the system acceptance. Hope this helps, Daniel Chartier |
Follow us on