1/30/2016 5:54 PM | |
Joined: 9/27/2006 Last visit: 9/1/2024 Posts: 12282 Rating:
|
Hello alsofi; The old_gsd screenshot shows an ident_number 00CF, whereas the gsd file for the Smartronic PC 1312 has an ident_number 051D. This is based on information in the following document: http://www.ksb.com/propertyblob/2104996/data - GSD file The SMARTRONIC PC unit GSD file (see appendix) is called 051D.GSD. The hexadecimal figure 051D corresponds to the SMARTRONIC PC Profibus identification number assigned by the PNO (Profibus Nutzer Organisation). When configuring the equipment corresponding to the unit, load file 051D.GSD. Then when selecting the data transfer modules, select Base module Please open the new gsd file for the PC 1312 and validate that the ident_number is different from the old_gsd. If that is the case you can install both gsd files in the Siemens configurator without problem, and use both positioners at the same time in the Profibus network. Hope this helps, Daniel Chartier |
Follow us on