11/18/2008 8:07 AM | |||
Joined: 9/27/2006 Last visit: 8/16/2024 Posts: 12277 Rating: (2680) |
Hello aym; This is the desription of your part numbers, from the A&D Mall:
That is the gsd file you need to use. You can find it here, if you do not already have it: http://support.automation.siemens.com/WW/view/en/113498 Hope this helps, Daniel Chartier |
||
11/18/2008 8:10 AM | |
Joined: 10/7/2005 Last visit: 8/9/2024 Posts: 3016 Rating: (1054) |
Dear aym_31 are you sure you have the correctpart number (to the best of my knowledge the numbers you listed don't exists in the Siemens world)? Anyway, the IM153-2 is part of the ET200M family and all IM153-xGSD files can be found here: http://support.automation.siemens.com/WW/view/en/113498 I hope this helps Nevermind my advise, D Chartier beat me to it (I have to learn to type faster ...) |
Last edited by: fritz at: 11/18/2008 8:12 AMCheers |
|
11/18/2008 10:32 AM | |
Posts: 37 Rating: (0) |
ok.. Now i get it Wizard. Thank u. |
11/18/2008 10:49 AM | |
Joined: 4/24/2006 Last visit: 8/16/2024 Posts: 8717 Rating: (1166) |
You are welcome Best regards, Wizard |
11/18/2008 11:29 AM | |
Joined: 4/24/2006 Last visit: 8/16/2024 Posts: 8717 Rating: (1166) |
Dear aym_31, Please have a look here: http://support.automation.siemens.com/WW/view/en/23372259 The change is because of change in order number IM153-2 Best regards, Wizard |
11/18/2008 11:49 AM | |
Joined: 4/24/2006 Last visit: 8/16/2024 Posts: 8717 Rating: (1166) |
Dear aym_31, Here is another link which indicates difference between IM153-2 high feature http://support.automation.siemens.com/WW/view/en/26291781 Best regards, Wizard |
Follow us on