2/4/2018 1:42 AM | |
Joined: 7/4/2010 Last visit: 3/17/2025 Posts: 5 Rating:
|
Hi all,
thanks |
2/4/2018 2:22 AM | |
Joined: 9/27/2006 Last visit: 3/16/2025 Posts: 12344 Rating:
|
Hello mzprx; See if the contents of this FAQ provides enough information to help you with your project: Combined configuration with WinCC (TIA Portal) and STEP 7 V5.x The gsdml/gsd files you are asking for are found below the video link. Hope this helps, Daniel Chartier |
Last edited by: Jen_Moderator at: 2/5/2018 12:23:14 PMOptimized link. |
|
This contribution was helpful to
3 thankful Users |
2/4/2018 5:33 PM | |
Joined: 1/21/2013 Last visit: 11/20/2024 Posts: 4620 Rating:
|
Hello, go under: Support Packages for TIA Portal V14 V14 HSP 0211 Support Packages for the hardware catalog in the TIA Portal (HSP) - ID ... |
Last edited by: Ste39 at: 2/4/2018 5:34:55 PMLast edited by: Jen_Moderator at: 2/5/2018 12:25:40 PMOptimized link. |
|
2/4/2018 11:30 PM | |
Joined: 9/27/2006 Last visit: 3/16/2025 Posts: 12344 Rating:
|
Hello mzprx; I hope I have understood your requirement. You want to use a PLC programmed in Step 7 v5.5 and access a number Comfort panels, programmed on Profinet with WinCC v14 SP1. You also wish to diagnose these panels and show the results in your WinCC v14 SP1 application. The following application note presents the tool that Siemens has developped for such a case (the example uses TIA Portal v13, but the principle should apply in your version): the device proxy *as shown in the screenshot belo2. Combined configuration with WinCC (TIA Portal) and STEP 7 V5.x By creating a Device Proxy in WinCC TIA Pôrtal, you allow exchanges between the PLC tags (generated in Step 7 v5.5) with the (comfort) panels in the WinCC v14 program. Here also an application note showing how to use PNIODiag:in the PLC: Diagnostic package PNIODiag for diagnostic evaluation for PROFIBUS DP and PROFINET IO (STEP 7 V5.x) Hope this helps, Daniel Chartier |
Last edited by: Jen_Moderator at: 2/5/2018 12:27:30 PMOptimized links. |
|
Follow us on