Industry Online Support
Technical Forum
7/13/2009 9:25 AM | |
Joined: 1/17/2007 Last visit: 10/6/2020 Posts: 289 Rating: (3) |
I have placed for you the diagnostic file. Most of the time the error is: Event 37 of 120: Event ID 16# 79E5 F-I/O passivated - Monitoring time exceeded at the safety frame detected in the F-CPU Logical base address: 56 F-I/O database number: 128 External error, Incoming event 11:01:32.481 AM 05/13/2008 I only start the system with all Profibus modules connected. Attachmentdownloadplc90710.pdf (136 Downloads) |
Follow us on