3/24/2024 8:44 PM | |
Joined: 5/24/2016 Last visit: 9/13/2024 Posts: 347 Rating: (52)
|
Hello. No you are not correct. It is processed in the PLC as to when and axis is to be controlled using the handwheel. That is what the WAND_B command is doing, it checks the input from the rotary switch and further down checks against the byte number as to which axis is active. It is a bit confusing if one is not used to this kind of programming. So here is and example I made where I use pure NO/NC logic to do the same thing. I hope it makes more sense with this simplified version. There are some extra features I always incorporate which means making changes to the MCP483 and MCP483_M block. These are - Traversing using + and - Keys also with Rapid Choose the Increment of the Axis using F1 for 1 - F2 for 10 and F3 for 100 Now I do not have a active system to test this on, so sorry if there is any bugs Best Regards Riddersholm
AttachmentMiniHHUExample.zip (195 Downloads) |
Follow us on