10/9/2020 6:24 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872)
|
Hello, 6FC5247-0AF08-5AA0 - SINUMERIK 40 GB SSD HARD DISK SSD WITH MOUNTING sutable for below PCU (WIN XP). 6FC5210-0DF52-2AA0 - SINUMERIK PCU 50.5-C 1,8 GHZ; 1 X 1024 MB RAM 24 V DC; WINDOWS XP PROFESSIONAL FOR EMBEDDED SYSTEMS (WINXP PRO EMBSYS) 6FC5210-0DF53-2AA0 - SINUMERIK PCU 50.5-P i5-520E; 2,4GHz; 1 x 2048MB RAM 24 V DC; WINDOWS XP PROFESSIONAL FOR EMBEDDED SYSTEMS (WINXP PRO EMBSYS) which id discountinued product & successor is 6FC5210-0DF53-3AA0. As far as HDD sale is considered, generally spare HDD are sold without software installed on it. From the MLFB, it is wthout software (compatible with WinXP PCUs). User can load data backup ghost/image file on spare HDD. In your case please confirm compatibility of above HDD with PCU you have. HTH. |
10/10/2020 4:56 AM | |
Joined: 10/17/2007 Last visit: 5/23/2024 Posts: 3991 Rating: (345)
|
Thanks for your answer. --can you make sure "As far as HDD sale is considered, generally spare HDD are sold without software installed on it. From the MLFB, it is wthout software (compatible with WinXP PCUs)" --where do you get this information. You know I search and found products in "Siemens automation mall" same description as you posted here. NO Clare description saying with or without SINUMERIK HMI Advanced Software installed. My question originally asked Siemens Customer support, but They did not give me the answer--I contact Forum Moderato for help forward to the Siemens Support Team, But She suggests Post in forum 1st to see I can get a confirmed answer. If not she will forward. The problem is Customer has No good Ghost/Image. also the 2nd hand machine most of the cases customers cannot get OEM support--I hope Siemens should consider this situation. in 2020, from June to last week,I have 3 customers who encountered a similar problem. the NCK is good, only the HMI HDD or SSD defective. This PCU50.5P is one of them. another 2 cases are MMC103 So I hope the information you provided is sure--I will not order an SSD without HMI software
|
If you like my comments please |
|
10/10/2020 5:17 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872)
|
Hello, I myself has procured spare HDD from Siemens without software. If user need particular software, end user should contact nearest Siemens service/support center along wth installed hardware, NCU, CF card, system software etc. etc. details, based on which Siemens will provide the solution. As you are aware, in Siemens automation, from time to time there are so many software Firmware versions, hardware upgradation, it requires to check/confirm compatibility issue, its very difficult to provide one line answer/solution . Even if end user has to face this problem & Siemens definately provides the solution if requiste data is submitted. Hope you also understand the same.
|
Last edited by: PISCEAN 2010 at: 10/10/2020 05:20:24 |
|
Follow us on