Industry Online Support
Technical Forum
11/7/2007 9:44 AM | |
Joined: 4/6/2006 Last visit: 2/5/2024 Posts: 604 Rating:
|
Hi Coach, This depends on what kind of features of the CP you are using. If you only use the regular communications (No ProfiNet) in combination with the CPU v5 there is no problem. If you need to use ProfiNet with a CPU v5 in combination with the 1EX40 this isn't possible. If you use a CPU v4 there in combination with the 1EX40 there is no problem at all. But ifyou want to use ProfiNet over the CP witha v5 CPU you need the 6GK7443-1EX41-0XE0. Good luck with it. By th way: SP3 for Step 7 isreleased already. Step 7 v5.4 SP3 Download |
Best regards, |
|
Follow us on