7/6/2009 3:10 AM | |
Joined: 12/20/2008 Last visit: 8/25/2022 Posts: 556 Rating: (236) |
Hi ZUMA, Please look at the informationhere. |
7/6/2009 3:37 AM | |
Posts: 62 Rating: (0) |
Hi Lalit, Nothing is there in your link. Isn’t it a “funny posting”? |
This contribution was helpful to1 thankful Users |
7/6/2009 3:42 AM | |
Joined: 12/20/2008 Last visit: 8/25/2022 Posts: 556 Rating: (236) |
Hi epro, Sorry, if you did not find the link, I was trying to provide the manual.
|
7/6/2009 4:27 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello ZUMA, Look at Which Engineering Software can be used with which panels?Uploading with WinCC Flex is only possible, if the Transfer of the current project file from the configuration computer to the operating unit must be performed using the Upload option "Enable backtransfer". About necessary (possible) cable look at What transfer options are available in the various operator panels? Hope this will helps. Best regards, |
This contribution was helpful to1 thankful Users |
Follow us on