2/2/2016 9:18 AM | |
Posts: 567 Rating: (107) |
Hi, did you use the PC as Engineering Station? I would say an SSD will give a better Performance. |
2/2/2016 1:14 PM | |
Posts: 25 Rating: (0) |
Hi, Computer model is Dell Poweredge R620. And we also have SSD but i think CPU performance is not good. |
2/16/2016 3:15 PM | |
Posts: 220 Rating: (11) |
Do you have installed PCS 7 on the SSD and save your Project on the SSD, too? I would agree to Ralfinio that a SSD gives you the best Perfomence improvement. Don't know if a better CPU would solve this. In the Readme from PCS 7 you can find the Information that the Hardware Requirement are the same as the from STEP 7. Here the link to the Requirement of STEP 7 5.5. |
Follow us on