10/19/2017 10:08 AM | |
Posts: 6 Rating: (1) |
Hi all, My question is related to this topic. I am using a high speed digital input 6ES7131-6BF00-0DA0 (8 X DI HS) in a ET200SP CPU. Has anyone used the oversampling mode or even the counting operating mode? Any program example about this? I didn't find anything in Siemens database. Thanks, Ricardo ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/19/2017 2:18:27 PMNew subject after splitting |
|
10/19/2017 3:27 PM | |
Joined: 9/27/2006 Last visit: 11/18/2024 Posts: 12294 Rating: (2691) |
Hello ferraz; To follow up on jacek d's judicious comment, here is an application example from Product Support discussing oversampling mode with the S7-1500; it contains a presentation document and a sample program that you can use to base your own project on: High-performance measurement technology in PROFINET environmentHope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
Follow us on