3/4/2020 11:07 AM | |
Joined: 2/4/2020 Last visit: 3/20/2024 Posts: 14 Rating: (0) |
in simulation, the program works fine. harware setup from left to right. was going to change inputs/outputs from the simulated program to its actual input/output... but i cannot see (or find?) modules in list? [snip] how do i know if i have selected Q1 on LOGO! 230RCEo or Q1 DM16 24R? AttachmentScreenshots.zip (194 Downloads) |
Last edited by: Jen_Moderator at: 03/04/2020 14:51:55Removed links and added files as an attachment. |
|
3/4/2020 11:55 AM | |
Joined: 1/21/2013 Last visit: 11/20/2024 Posts: 4620 Rating: (709) |
Hello ixo, Q1-Q4 ? |
3/4/2020 1:44 PM | |
Joined: 12/18/2014 Last visit: 1/26/2025 Posts: 34557 Rating: (4314)
|
Sure... Fingers faster then the head |
Follow us on