12/8/2017 2:14 PM | |
Joined: 11/21/2016 Last visit: 6/23/2022 Posts: 3 Rating: (0) |
Hello All I am having trouble loading a program from a sd card to the logo. I am using the correct update software, the card is already formatted, I am using the file LOGO_U_P.BIN . I put the card in with logo off and then with the logo on, still it will not see the program. Once it load half a program in to the logo but since then nothing will load in. Can anyone tell me what I might be doing wrong I have read and acted on the posts in the forum but nothing has worked for me so far. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/11/2017 9:11:23 AMNew subject after splitting |
|
Follow us on