6/10/2011 11:25 AM | |
Joined: 11/18/2010 Last visit: 8/5/2022 Posts: 523 Rating:
|
hi, first specify,which protocol your HMI support.then we can check communication possibility. viral patel
|
6/10/2011 11:28 AM | |
Joined: 4/19/2008 Last visit: 11/21/2024 Posts: 1525 Rating:
|
Hi Thunder, As per the Product HMI IDEC HG2G is only Support the S7-200 PLC App Note: Siemens S7-200 CPU 212 It is look like from the above link. & I can't able to find the Detail About V806CD HMI |
Last edited by: Ammy at: 6/10/2011 11:32 AMV806CD Detail Ammy |
|
This contribution was helpful to
1 thankful Users |
6/10/2011 11:34 AM | |
Posts: 241 Rating:
|
Dear Thunder, Please see the Manual, Ch24 for Siemens PLC connection with MONITOUCH hmi. Manual is very clear. This HMI suports MPI Protocol which is easier for you to connect, and make your own MPI cable as wiring diagram also given in the manual. |
Last edited by: PowerTags at: 6/10/2011 11:36 AMfew wrds |
|
6/10/2011 11:43 AM | |
Posts: 38 Rating:
|
Dear all! can you point me in the HMI can be connected to the CPU 313c 2DP? Thank you! |
6/10/2011 12:00 PM | |
Posts: 38 Rating:
|
Hi Ammy! I found the connection diagrams in the documentation of HMI HG2G But can't connection. You can explan to me? Thank You! As per the Product HMI IDEC HG2G is only Support the S7-200 PLC App Note: Siemens S7-200 CPU 212 It is look like from the above link. & I can't able to find the Detail About V806CD HMI AttachmentHost_IF_E.pdf (104 Downloads) |
6/10/2011 12:18 PM | |
Joined: 4/19/2008 Last visit: 11/21/2024 Posts: 1525 Rating:
|
Hi thunder, S7-200 PPI port, S7-200 PLC HMI Side 3 6 & 8 8 7 & 9 If you want to Communicate the S7-300/400 PLC then you have to used the CP 340 or CP341 (RK512 & 3964R Protocol ) Card for the Communication, I can say don't go with this option, it is slower & expensive & for MPI port Checked 5.2.3 Chapter, HG1F Connection on Page No 4. & I have not worked on this HMI so you have to do the Some try out on your Side. if you have any problem I can Help you on based on Manual |
Ammy |
|
Follow us on