8/16/2018 5:10 PM | |
Posts: 6 Rating:
|
Hello Guys, My project is to do positioning using Sinamics, DCM drives on profibus. We are using S7-1500 controller and DriveLib V51 library blocks from this link: DriveLib Blocks My problem is I can do the commissioning (speed, jog, positioning) using technology objects > commissioning features but can't do the same using blocks from library above. Error I get is 16#8402, which says "Switching-on inhibit" Find test backup in here: Test backup I am using TIAV15 Upd 2 and no additional softwares. Stuck on this, AttachmentKnives_test_20180816_1600.zip (202 Downloads) |
Last edited by: Jen_Moderator at: 8/17/2018 9:57:55 AMOptimized link. Added Test backup as an attachment. Last edited by: Jen_Moderator at: 8/17/2018 9:58:21 AMRemoved link from Test backup. |
|
8/17/2018 5:18 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating:
|
Have you referred SINAMICS DCC: Positioning and synchronism with SINAMICS DCM and CU320-2 |
Last edited by: Jen_Moderator at: 8/17/2018 9:55:48 AMOptimized link. |
|
8/17/2018 9:32 AM | |
Posts: 6 Rating:
|
No, I am not using Starter with TIA Can't I just use DriveLib51 and do it? Manual says its possible and I have followed it but still stuck with 16#8402 and its not moving |
8/17/2018 2:55 PM | |
Posts: 6 Rating:
|
Solved.. used Technology objects functions instead of this library |
Follow us on