11/8/2016 9:43 AM | |
Posts: 19 Rating: (0) |
Good day. Help solve the problem of setting up a connection between WinCC 7.2 and the S7-1200. The server is installed SCADA WinCC 7.2 + Upd 9 and Simatic Net v8.2 SP1. Set up multiple connections to the S7-300, to which the questions asked, and one connection to the S7-1200, it does not work. At the facility is CPU-1215C controller (6ES7215-1HG40-0XB0). firmware version 4.1. On the part of the controller can ping the server. With a laptop, on which the TIA Portal V13 SP1, Step7 remotely connected and goes online with no problems, and connect WinCC does not want to. In WinCC 7.2 added standard driver "SIMATIC S7-1200. S7-1500 Chanel", it created a connection to the parameters as shown in the attachment. The Simatic Net interface PG / PC is configured. When WinCC is started, the connection to the S7-1200 gives the status of "the Disconnect", and accordingly the value of tags in the picture in runtayme not appear, although the compounds with the S7-300 controllers, with the status "OK". The controller in the network settings added station "Simatic PC station", it added communication module "IE general" and "Application" module. The module "IE general" all necessary network settings on display. The module "Application" a version of the software "Simatic Net PC software v8.1 SP2". It seems all right, but does not work, tell me which way to dig further.
AttachmentWinCC 72 and S7-1200.pdf (904 Downloads) |
11/9/2016 8:20 AM | |
Posts: 19 Rating: (0) |
Hello, in the file when the project starts in the Runtime continuously recorded one and same message. The last two entries in the file: 2016-11-09 12:05:46,758 INFO Log starting ... 2016-11-09 12:05:46,758 INFO | LogFileName : C:\Program Files (x86)\Siemens\WinCC\Diagnose\CCS7PlusChannel_01.LOG 2016-11-09 12:05:46,758 INFO | LogFileCount : 3 2016-11-09 12:05:46,758 INFO | LogFileSize : 1400000 2016-11-09 12:05:46,758 INFO | TraceFlags : c4000000 2016-11-09 12:19:20,355 INFO Log starting ... 2016-11-09 12:19:20,355 INFO | LogFileName : C:\Program Files (x86)\Siemens\WinCC\Diagnose\CCS7PlusChannel_01.LOG 2016-11-09 12:19:20,355 INFO | LogFileCount : 3 2016-11-09 12:19:20,355 INFO | LogFileSize : 1400000 2016-11-09 12:19:20,355 INFO | TraceFlags : c4000000 Attached log file, If I understand correctly, in the log file does not contain errors. AttachmentCCS7PlusChannel_01.txt (526 Downloads) |
Last edited by: mr_ovchinnikov at: 11/9/2016 9:18:37 AMLast edited by: mr_ovchinnikov at: 11/9/2016 9:21:17 AMLast edited by: mr_ovchinnikov at: 11/9/2016 9:21:38 AM |
|
11/9/2016 9:37 AM | |
Joined: 4/28/2015 Last visit: 4/17/2024 Posts: 11 Rating: (3) |
WinCC Connection to S7-1500, S71200 and ET 200SP
This post shows you how to use the " SIMATIC S7-1200 , S7-1500 Channel " a connection between an S7-1500, S7-1200 or ET200SP and WinCC V7.3 SE. Task Functions
Documentation |
This contribution was helpful to1 thankful Users |
11/10/2016 5:31 AM | |
Posts: 19 Rating: (0) |
Hello, I'm doing the same thing, just add tags manually. See attached file. What am I doing wrong, tell me, please. AttachmentWinCC 7.2 and S7-1200.pdf (792 Downloads) |
Follow us on