11/16/2012 6:19 PM | |
Joined: 11/16/2012 Last visit: 9/3/2024 Posts: 10 Rating:
|
I think you need software from Siemens called "SIN805PC" to do what it would make the "Siemens Keyboard". This software runs on a PC and you need a PCIN communications cable on interface 2 (or interface 1, I´m not remember so well). You need to put start-up switch in position 2 (normally it is at position 0). With this software I suppose that you probably be able to format CNC and to input NC parameters, PLC parameters, PLC program by the other port or interface. I think that you need two PC´s or laptops with COM ports. ¿Have you got the backup of this machine (tea1, tea2, sea, etc) ?
|
1/7/2018 12:15 PM | |
Joined: 9/1/2005 Last visit: 1/28/2025 Posts: 4114 Rating:
|
New questions published by guardiano are split to a separate threads with the subject The sin805pc software, where can I find it? and Help sinumerik 805 - cable for data transmission. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on