1/4/2021 8:04 PM | |
Joined: 2/24/2020 Last visit: 5/18/2022 Posts: 7 Rating:
|
Sorry, my bad. I mean lower! |
1/4/2021 8:14 PM | |
Joined: 12/18/2014 Last visit: 7/27/2024 Posts: 33421 Rating:
|
I hope I have you understand correct. You didn't write which LOGO! device you exactly have. That's the reason why I made the program for a 0BA8.Standard. AttachmentPressure+speed_control_0BA8.Standard.zip (148 Downloads) |
1/4/2021 8:21 PM | |
Joined: 12/18/2014 Last visit: 7/27/2024 Posts: 33421 Rating:
|
Hello rickmoerman, you're welcome ... |
This contribution was helpful to
1 thankful Users |
1/5/2021 10:27 AM | |
Joined: 2/24/2020 Last visit: 5/18/2022 Posts: 7 Rating:
|
Hello Goodmorning everyone, I upgraded it. I have another question. If the pressure sensor is broken, so the value falls below 4 mA, then output Q1 and Q2 should not switch. how do i make this? AttachmentOil Protection.zip (142 Downloads) |
1/5/2021 10:31 AM | |
Joined: 12/18/2014 Last visit: 7/27/2024 Posts: 33421 Rating:
|
There is only a shortcut to the file in the folder. The file itself is missing. |
Follow us on