10/7/2016 3:13 PM | |
Joined: 11/14/2008 Last visit: 5/6/2024 Posts: 504 Rating: (22) |
As far as I can see you have an error class 5 , which is caused by next issue as explained in manual. Please check your hardware ... Look if you've added correct module by checking MLFB,check Firmware etc... 5 Error in hardware interrupt setting Cause: You have attempted to select a hardware interrupt that the module does not support. Attachments7300_fm352_ErrorMessages.pdf (186 Downloads) |
Follow us on