Industry Online Support
Technical Forum
8/19/2013 5:57 PM | |
Joined: 1/28/2009 Last visit: 10/11/2024 Posts: 6852 Rating: (1365)
|
Hello, That is also possible easily in SCL: [code] ORGANIZATION_BLOCK OB1 VAR_TEMP // Reserved info : ARRAY[0..19] OF BYTE; // Temporary Variables END_VAR // Statement FOR LP:= 0 TO 99 BY 1 DO // Statement Section ; IF (0 <= LP) AND (LP < 5 )THEN ; TEST.T[LP]:=1; ELSE TEST.T[LP]:=0; ; END_IF; ; END_FOR; ; END_ORGANIZATION_BLOCK[/code] As I remember, we discussed the same issue before but I should search for that to find.The most compelete set of samples on indirect addressing of arrays can be found here for a really complex example in both SCL and STL: Arrays, DB and pointersBest regards Hamid Hosseini |
Follow us on