2/27/2018 9:07 PM | |
Posts: 4 Rating: (0) |
Hello everybody :) I am home studying plc programming - And i am writing a small program.. But i now i have a SF Fault and i reelly cant find out of why.. I have uploaded my program .. i contains 4 FC and 4 DB - so if any one have the intereest of helping me it could be nice :) I think the problem is something with the FC called "Weight" - When its not called in the OB1, then no problem. The problem will come, when I5.4, I5.1, I5.3, I5.5 is high (Starts the Automatic mode).. BTW the program is not near finish jet AttachmentProject.zip (35 Downloads) |
Last edited by: Majlund88 at: 2/27/2018 9:08:12 PMLast edited by: Majlund88 at: 2/27/2018 9:09:17 PM |
|
2/27/2018 11:48 PM | |
Joined: 11/5/2012 Last visit: 8/10/2024 Posts: 487 Rating: (63) |
Hello Majilund88. I'll leave a document that illustrates what process image is and also a this link to a FAQ discussing the peripheral addressing. I hope this information will help you to clear your doubts and understand how to use peripheral and PI addressing in the best way. Regards. Edit: I see that on TIA is a little bit different but the principles should remain the same. AttachmentProcess Image.pdf (44 Downloads) |
Last edited by: Rescobedo at: 2/27/2018 11:49:55 PMLast edited by: Jen_Moderator at: 2/28/2018 10:51:53 AMOptimized link. |
|
Follow us on