Industry Online Support
Technical Forum
6/10/2010 6:51 PM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (836) |
Hello Galo003789, You have 5 CPUs connected to each other via profibus network. And each CPU is connected to an OP270 via MPI. So, for CPU1: Suppose that its MPI address is : 2 and OP270 MPI address is 1. The same for the other CPUs because you have 5 different MPI networks. So, why you want to change the MPI address of the OPs?! you do not need to change it. In any case, without the project (i.e. CS project of OP270), you won't be able to change the address. |
Ayman Elotaify |
|
6/10/2010 8:01 PM | |
Joined: 8/27/2006 Last visit: 4/23/2024 Posts: 719 Rating: (88) |
I want to help with an idea. The question for Ayman: is it possible forGalo003789to use any sort of DP/DP coupler or a DP gateway so that every CPU+HMI is isolated in a sub network?
then he can communicate every subnetwork with the other ones? |
Last edited by: AMAZINGAHMED at: 6/10/2010 8:02 PMThe more you know, The more you know that you don't know |
|
Follow us on