1/3/2007 1:40 PM | |
Joined: 9/28/2005 Last visit: 12/14/2022 Posts: 414 Rating:
|
Am I correct when I conclude that you don't have STEP7 programming software? Is there any SF-led on? On a module or on the CPU? See also the manual S7-300Automation System Module data for more information. You can find it at this link. See also the manual S7-300 Automation System, Hardware and Installation: CPU 312IFM - 318-2 DP at this link. |
Smurf |
|
1/3/2007 2:07 PM | |
Joined: 9/28/2005 Last visit: 12/14/2022 Posts: 414 Rating:
|
When only the battery led is on I and your system will not go in Run then I think the program memory in the CPU is cleared. Do you have a backup of the program on e.g. a memory card? If so, you can place the memory card in the CPU and have a power up. If not you can ask your supplier for a memory card with the software. If you are using a memory card without a battery all settings are lost every time youswitch off the CPU, having placed a battery the RAM is still powered and settings are kept. To be sure you can add a battery replacement (CPU must be switched on) in the yearly mainenance instructions thendown times are reduced. Having typed this information I remembered that Siemens has a link for downloading a free version of STEP7 Lite V3.x at this link. After installing this on your computer or notebook you only need a PC adapter USB (6es7 972-0cb20-0xa0) for programming/monitoring. Now you can make abackup of the software as well. |
Smurf |
|
1/7/2007 2:47 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating:
|
[quote user="Smurf"]When only the battery led is on I and your system will not go in Run then I think the program memory in the CPU is cleared. Do you have a backup of the program on e.g. a memory card? If so, you can place the memory card in the CPU and have a power up. If not you can ask your supplier for a memory card with the software. If you are using a memory card without a battery all settings are lost every time youswitch off the CPU, having placed a battery the RAM is still powered and settings are kept. To be sure you can add a battery replacement (CPU must be switched on) in the yearly mainenance instructions thendown times are reduced. Having typed this information I remembered that Siemens has a link for downloading a free version of STEP7 Lite V3.x at this link. After installing this on your computer or notebook you only need a PC adapter USB (6ES7972-0CB20-0XA0) for programming/monitoring. Now you can make abackup of the software as well. Hi Smurf, A very good answer ! |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on