5/29/2015 4:56 PM | |
Joined: 12/18/2014 Last visit: 7/27/2024 Posts: 33421 Rating:
|
Which logo do you have? 0BA8? or 0BA7? |
5/29/2015 4:58 PM | |
Joined: 12/27/2006 Last visit: 7/7/2024 Posts: 1197 Rating:
|
You can also programm the LOGO in ladder. And if you have make a programm in ladder LOGOSoft automaticaly can make it to FBD (and also FBD to ladder). There is a button for it in LOGOSoft Comfort. I can advise you to make all your programms in FBD. In FBD you can more, the programm is much litteler. You can plase much more on 1 sheet and can see al the connections etc.
Use a a-syncron pulsmaker and a couter. And from the input use a RS blo, that reset whet the counter is 3 In the attachment a example. Its not perfect, What happens if you constantly press the doorbell? You can make somethin to it. Adjust the plsgenerator B002 AttachmentCircuit Diagram1.zip (156 Downloads) |
Last edited by: Toeternietoe at: 5/29/2015 5:05:09 PM |
|
5/29/2015 5:02 PM | |
Posts: 3 Rating:
|
0BA6 |
5/29/2015 6:24 PM | |
Joined: 12/18/2014 Last visit: 7/27/2024 Posts: 33421 Rating:
|
Hello Phil-A, possible you like this. |
Follow us on