Industry Online Support
Technical Forum
1/16/2011 3:02 PM | |
Joined: 1/28/2009 Last visit: 7/5/2024 Posts: 6841 Rating: (1361) |
Two well known options are: 1-PLC-ANALYZER pro 5 2- ibaPDA Wincc from SIEMENS also provide data aquisition of at least 500ms in normal cases(e.g in S7300).If I do not have those Softwares I assign a counetr for each of switches(N.O) and monitor the values.If you switches are N.C use a Not command before the counter. BR |
This contribution was helpful to2 thankful Users |
Follow us on