8/9/2017 9:31 AM | |
Joined: 7/19/2016 Last visit: 4/19/2022 Posts: 5 Rating:
|
Dear Sir, I had attached photo of HMI problem, Please help me to resolve the problem. 1.After giving power cycle that pop is showing. 2.In TIA Portal HMI was not detect. 3.Also Using S7, Edit Ethernet Node MAC Address was not detect. I want to Update OS or Reset Factory Setting, How should i remove that pop up or Detect that HMI in TIA Portal?
|
8/9/2017 9:45 AM | |
Joined: 4/24/2006 Last visit: 3/14/2025 Posts: 8894 Rating:
|
Hello, Perhaps you can try to use Prosave to perform an OS update: Prosave is installed on your pc. Or you can download: Best regards, Wizard |
This contribution was helpful to
1 thankful Users |
9/21/2017 1:02 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating:
|
New question published by klllll is split to a separate thread with the subject After clicking update button error message "No connection could be established. Please verify your settings, interfaces, cables, device type etc" occurs.. Best regards |
Follow us on