8/20/2018 8:43 AM | |
Posts: 10 Rating: (0) |
Hello, Recent am working with Siemen Simatic HMI MP277 6" and 12" HMI, the issue we facing the 12" HMI not communicating with 12" HMI. I check all the parameter in machine HMi but no luck. basically the machine has to work with remote mode but in case option the HMI not letting insert any valve on 12" HMI. rest 6" HMI working in local mode, let me know what i can do to make it work on remote mode. Regards, Manish Sharma ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 8/20/2018 10:15:19 AMNew subject after splitting |
|
8/20/2018 10:17 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice.
|
Follow us on