10/19/2016 5:35 PM | |
Joined: 6/4/2010 Last visit: 5/3/2024 Posts: 376 Rating: (126)
|
Dear Mads, You need a PXM20 (-E) operator unit. This is a plug and play device. The PXM20 (-E) operator unit reads all the controllers with all the data points available and list them in a structured form. PXM20 is for LON networks, PXM20-E is for BACnet on IP networks. Operating functions: Further information can be found under the following link: Best regards, |
Follow us on