Industry Online Support
Technical Forum
3/31/2014 6:53 AM | |
Posts: 7 Rating: (1) |
dear all, I work on one project where i need to translate all project ENGLISH to FRENCH i change almost 99.99% project using language settings. the problem is that when there is say eg. "25.5" in io field when we open french screen it shows "25,5" give me solution for that hmi is KTP 1000 BASIC COLOR PN thanks.... Regards, Attachmentupload.zip (38 Downloads) |
Last edited by: sssonawane at: 3/31/2014 6:55 AM |
|
3/31/2014 8:57 AM | |
Posts: 7 Rating: (1) |
Dear all, software is wincc flexible2008 service pack sp3 |
3/31/2014 10:51 AM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hi Same problem ???? hmi problem |
3/31/2014 1:44 PM | |
Joined: 9/1/2005 Last visit: 3/5/2024 Posts: 4097 Rating: (193) |
closed cause question discussed twice. The second thread with the subject hmi problemis published within the same conference. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on