2/28/2019 11:56 AM | |
Posts: 3 Rating:
|
Good morning We have some doubts about the installation of HMI TP700 Comfort in hazardous area Class 1, Zone 2, Group IIB, T3, IP65 in the specifications on the siemens site it reports that the operator panel is certified for this area, and the only caution is that being the rear side certified only IP20 (while the front is ip66) must be placed in an IP65 enclosure for our applications (for example we found a polyester/fiberglass ip66 enclosure with transparent front door from Gewiss).
|
Last edited by: Stirome at: 2/28/2019 11:57:39 AMLast edited by: Stirome at: 2/28/2019 11:57:57 AMLast edited by: Stirome at: 2/28/2019 12:08:46 PMLast edited by: Stirome at: 2/28/2019 12:09:22 PMLast edited by: Stirome at: 2/28/2019 12:10:17 PM |
|
3/4/2019 3:48 PM | |
Posts: 3 Rating:
|
So no one know if this HMI is suitable for Class I Zone 2 ? I've spoken with siemens support also, and they reply that they simple read what is written in the datasheet |
3/5/2019 3:53 PM | |
Joined: 10/19/2005 Last visit: 11/30/2020 Posts: 1611 Rating:
|
Hey, can you tell us where you have read that a TP700 Comfort could be use in an hazardous area I mean this is not possible without further ado! Look to this FAQ =>https://support.industry.siemens.com/cs/ww/en/view/291285 There are only talk about area zone 2/22 and if you read the download file Conditions of use for Zone 22 I mean a colleague from me use a casing from "BARTEC" and he get infos from "BARTEC" what he has to do...! They are the right specialists for this. regards, |
3/6/2019 3:58 PM | |
Posts: 3 Rating:
|
Thank you for the reply. Class 1 Zone 2 compliance is indicated in the datasheet and I 've found also a certificate on the site. Moreover in the link you have posted is shown the nameplate for a TP900 that reports Class 1 zone 2 Group A, B,C, D T4. The only issue is the IP 66 certification for the front and IP20 for the rear of the panel that we understand implied the HMI to be installed in a IP66 enclosure. |
Last edited by: Stirome at: 3/28/2019 2:58:56 PM |
|
6/17/2020 8:11 PM | |
Posts: 1 Rating:
|
The typical way this is used is to install it in a control enclosure that is purged and pressurized with inert gas, like air. When done correctly this makes the interior into an unclassified location. The IP rating is not related to the hazardous location data. |
We are working on a new user interface with better overview and more relevance.
Follow us on