4/9/2024 5:38 AM | |
Joined: 5/12/2006 Last visit: 6/13/2024 Posts: 22263 Rating: (2989) |
and which error exactly? Have you configure the hmi device in the project as V15 device? |
4/9/2024 5:44 AM | |
Joined: 5/12/2006 Last visit: 6/13/2024 Posts: 22263 Rating: (2989) |
screen of the error please! |
4/9/2024 5:59 AM | |
Joined: 3/18/2024 Last visit: 6/12/2024 Posts: 27 Rating: (0) |
|
4/9/2024 6:12 AM | |
Joined: 5/12/2006 Last visit: 6/13/2024 Posts: 22263 Rating: (2989) |
Install the panel images from dvd3/4 and the error is fixed |
This contribution was helpful to2 thankful Users |
Follow us on