12/23/2010 12:53 PM | |
Joined: 4/14/2010 Last visit: 4/3/2024 Posts: 525 Rating: (11) |
Can you suggest Order number for DP/DP Coupler...??? |
MS |
|
12/23/2010 2:09 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Configuration of the I/O Data on DP/DP Coupler What are the special features of input/output addressing with the DP/DP coupler? DP/DP Coupler manual Best regards, Hristo Mihalev |
12/23/2010 3:55 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Note! Max. data lengthin in this way is limited up to 76 bytes. Best regards, Hristo MIhalev |
12/24/2010 10:39 AM | |
Joined: 7/2/2008 Last visit: 4/5/2024 Posts: 928 Rating: (305)
|
Hello Sarfraz Bhatti, You don't need any additional hardware and just for your information there's no DP/DP coupler with three Master lines (ports). You can build a simple network as attached. All you need is Profibus cable and some suitable bus connectors and then it should work. Check this link to know how to build a connection between a panel and a single CPU. You can use the same procedure with the other 2 CPUs. Best regards. H-H |
This contribution was helpful to1 thankful Users |
Follow us on