4/25/2023 11:13 AM | |
Joined: 3/30/2014 Last visit: 8/8/2023 Posts: 83 Rating: (0) |
So far I have all LOGOs on point. But now some errors are popping up with the HMI. Mainly with the LOGO "roller blinds" and displaying on the HMI. When I select bedroom 1, CLOSE lights up. bedroom 2 -> bedroom 1 Dining room -> bedroom 2 terrace east -> Dining room terrace south -> terrace east terrace south does nothing TV corner, kitchen and central is ok. Then when I press "close" then "open" lights up. And when "open" nothing happens. Errors in the HMI tag table? Don't know. It's possible, but don't see it. KTP 700 Basic 6AV2 123-2GB03-0AX0 AttachmentLogo Hoefsmid.zip (319 Downloads) |
4/25/2023 11:30 AM | |
Joined: 3/30/2014 Last visit: 8/8/2023 Posts: 83 Rating: (0) |
AttachmentTranslate.xlsx (245 Downloads) |
4/25/2023 11:59 AM | |
Joined: 12/18/2014 Last visit: 5/17/2024 Posts: 33050 Rating: (4082)
|
and so on .... See attachment ... AttachmentTags_LOGO!--TIA.zip (352 Downloads) |
Last edited by: ixo65 at: 04/25/2023 11:59:55 |
|
Follow us on