7/5/2019 5:41 PM | |
Joined: 9/27/2006 Last visit: 5/19/2024 Posts: 12257 Rating: (2668)
|
Hello Hich_IO; That specific hotfix is quite old, and Step 7 v5.4 has been replaced first by Step 7 v5.5, now by Step 7 v5.6. Hotfix 4 for Step 7 v5.4 SP5 is no longer available on the Product Support. One option is to do a support request (the link is at the top of this page) and ask Siemens techs to provide the file; I doubt that they will have it on hand, and they might simply suggest to purchase a Step 7 v5.5 (or 5.6) license, which includes all the modifications and HSPs from preceding versions. Or you might have a look into this support download: STEP 7 V5.x Hardware Support Packages (HSPs - as at 06/2019) for installing hardware updates in the Hardware Configuration https://support.industry.siemens.com/cs/ww/en/view/23183356 Hope this helps, Daniel Chartier |
7/5/2019 7:22 PM | |
Posts: 10 Rating: (0) |
Thank you for your answer, I really appreciate it, I have already downloaded the last hardware update contained the CP-342-5 6GK7 342-5DA03-0XE0 in the Hardware Configuration (https://support.industry.siemens.com/cs/ww/en/view/23183356) but I couldn't copy the requested module CP-342-5 6GK7 342-5DA03-0XE0 to my catalog. I have the Step 7 V5.4 SP5 and I need to install the HotFix4 for STEP7 V5.4+SP5 the problem the old CP-342-5 6GK7 342-5DA02-0XE0 is defected and we are facing the process destabilization. Is there any other way to download this .exe file? Thank you, Hich_IO |
7/8/2019 1:00 PM | |
Posts: 10 Rating: (0) |
Many thanks for your support, Siemens support provided me with the required file and Issue was fixed, HBenK |
This contribution was helpful to1 thankful Users |
Follow us on