7/25/2021 5:30 PM | |
Joined: 6/7/2020 Last visit: 2/22/2024 Posts: 3 Rating:
|
please, i have the same problem, I tried to setup Protool V6SP3, I have windows 10 on my pc, when I started the setup I find an error the " operating system does not support " how I can change from the setup file of prolool the operating system to windows 10 ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/26/2021 11:49:35New subject after splitting |
|
7/25/2021 5:51 PM | |
Joined: 12/18/2014 Last visit: 8/7/2024 Posts: 33504 Rating:
|
Not possible. |
7/25/2021 8:05 PM | |
Joined: 9/27/2006 Last visit: 8/7/2024 Posts: 12273 Rating:
|
Hello; You should think in terms of installing a VM with a Windows OS that figures in the supported list of ProTool v6.0 SP3, as shown in the screeshot below. This list was taken from the followong Product Note: https://support.industry.siemens.com/cs/ww/en/view/19962184 Please note also thr versions of Step 7 that can be installed with ProTool v6.0 SP3, in the same document. Hope this helps, |
Follow us on