10/29/2020 1:57 PM | |
Posts: 1 Rating: (0) |
BONJOUR SVP DIT MOI COMMENT TELECHARGER LE LOGITIEL S7 PLCSIM V5.5 MERCI ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/30/2020 06:46:30New subject after splitting |
|
10/29/2020 10:09 PM | |
Joined: 9/27/2006 Last visit: 8/6/2024 Posts: 12273 Rating: (2680) |
Bonjour Politive; Comme Hati vous l'a fait remarquer, le forum de Siemens a décidé d'utiliser l'anglais comme langue internationale, car le forum attire des participants du monde entier, et nos échanges en sont facilités. Svp utilisez l'anglais lors de votre prochaine visite. Notez que la plupart des documents que vous trouverez sur ce site (dit SIOS, Siemens Industry Online Support) sont disponibles en plusieurs langues, dont le français. Voyez l'image ci-dessous. Hello Politive; As Hati has already noted, The Siemens forum has chosen to use English as an international language, it makes our exchanges easier when you have participants from the wold over. Please write to us in English when you visit us again. Note that most documents that can be found on the site (called SIOS, Siemens Industry Online Support) can be opened in various languages, including French. Refer to the screenshot below. Now, it seems that the latest version of Step 7 PLCSim (for Step 7 v5.5) is PLCSim v5.4 SP8. You can download a trial version, fiully functional for 21 days, from this link. After the runtime period is over, if you want to continue using it, you are expected to purchase a license for the software. https://support.industry.siemens.com/cs/ww/en/view/109750064 Hope this helps, Daniel Chartier |
This contribution was helpful to2 thankful Users |
Follow us on