5/30/2014 8:00 AM | |
Joined: 11/21/2007 Last visit: 7/7/2024 Posts: 2325 Rating:
|
Hello friends Here is some information regarding a few prominent pillers of the Forum which will give you some idea of what effort is required for becoming Sliver / Gold / Platinum / Diamond Members UMENCHO - Posts : 9770 , Ratings : 1027 , Level : Diamond hdhosseini - Posts : 4417 , Ratings : 657 -Level : Platinum + 4 Bars
IBN-Service- Posts : 6013 , Ratings : 591 - Level : Platinum + 4 Bars fritz - Posts :2498 , Ratings :685 - Level : Platinum + 4 Bars J_Bell- Posts :5820 , Ratings :365 - Level : Platinum +3 Bars Marcjan- Posts :4692 , Ratings : 465 - Level : Platinum +3 Bars Ayman Elotaify - Posts :3145 , Ratings : 575 - Level : Platinum +2 Bars huggy_d1- Posts : 2771 , Ratings : 306 - Level : Platinum + 1 Bar Ekalavya- Posts :2721 , Ratings :422 - Level : Platinum +1 Bar Vithani - Posts :1795 , Ratings :442 - Level : Platinum Amit_86- Posts :1725 , Ratings :226 - Level : Platinum PISCEAN 2010- Posts :1664 , Ratings :78 - Level : Platinum Ammy - Posts :1467 , Ratings :133 - Level : Platinum playerslight- Posts :982 , Ratings :56 - Level : Platinum H-H- Posts :740 , Ratings :201 - Level : Platinum The list is by no means complete, but an indication of the effort required to be put in to reach these levels. Sure a lot of hard work and dedication, besides the commitment to share your knowledge to help others is needed to reach these levels. Hats off to all of you above and also those i forgot to list .. Well .. this is the data at the time of writing this post .... the count would have increased by the time you read it Cheers Navnag |
Last edited by: Navnag at: 5/31/2014 8:24 AMH-H and Fritz added Last edited by: Navnag at: 5/30/2014 6:31 PMLast edited by: Navnag at: 5/30/2014 10:04 AMplayerslight added Last edited by: Navnag at: 5/30/2014 9:19 AMFritz Added Last edited by: Navnag at: 5/30/2014 8:00 AMSpell Check There is no such thing as the last bug in a program |
|
This contribution was helpful to
2 thankful Users |
5/30/2014 2:21 PM |
|
Joined: 5/28/2013 Last visit: 2/1/2023 Posts: 112 Rating:
|
Great list! About the fritz is such an outstanding expert with very accurate answers and playerslight helps a lot to, with nice answers but isnt an expert..
|
5/30/2014 5:53 PM |
|
Joined: 11/21/2007 Last visit: 7/7/2024 Posts: 2325 Rating:
|
Great list! About the fritz is such an outstanding expert with very accurate answers and playerslight helps a lot to, with nice answers but isnt an expert.. Hello BBPrudente fritz - has earned the Platinum + 4-Bars with almost half the no of Posts :2498compared to others in the same league( hdhosseini: 4417,IBN-Service: 6013 ) playerslight- too has reached Platinum level with much lesser no of posts than others in the same league Posts :982 ( Vithani:1795, Amit_86:1725, PISCEAN 2010:1664, Ammy: 1467) These probably aretribute tothe quality of his posts. Cheers Navnag |
There is no such thing as the last bug in a program |
|
5/30/2014 5:56 PM | |
Joined: 7/7/2010 Last visit: 7/17/2024 Posts: 14970 Rating:
|
I could not agree more that fritz and playerslight have greatly contributed in different and unique ways. Congrats! |
science guy |
|
This contribution was helpful to
2 thankful Users |
5/30/2014 7:06 PM | |
Posts: 8946 Rating:
|
Both guys are here for a long time and do posts from very high quality. And Fritz is one offbest members here anyway. That will be the reason for the high level that they have earned honestly. |
This contribution was helpful to
2 thankful Users |
Follow us on