9/27/2023 11:51 AM | |
Joined: 9/27/2023 Last visit: 10/2/2023 Posts: 2 Rating: (0) |
Hello, dear experts, I have a process that is a combination of several types of substances, and the percentage of injection is determined by the operator, and every valve is opened and closed at the right time. How can I change the order of these materials so that the operator can change the opening and closing order of each valve according to the new formula? For example 1>2>3>4 replace with 1>2>4>3 And the sequence of opening and closing of these valves can be selected as desired
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/28/2023 08:43:40New subject after splitting |
|
10/2/2023 3:33 PM | |
Joined: 9/27/2023 Last visit: 10/2/2023 Posts: 2 Rating: (0) |
Thanks for your help, what logic can be used to create this chart? |
Follow us on