11/29/2016 2:30 PM | |
Posts: 16 Rating: (0) |
Dear sir I have a cnc machine. The power moduLe of spindeL is SEIMENS with order NO:6SN1135-1BA12-0DA0 Power moduLe has probLem,I repLace that with new type with order NO:6SN1123-1AA0-0DA1. ControL unit order NO is:6SN1121-0BA11-0AA1,after power on aLways I have F-17 on Lcd controL unit and some times F-79 I try to change values p-95 from 1 to 7 for reset the fauLt, but I cant beacuse code No new power moduLe is 7 but Icant change vaLues p-095. How can I change vaLues p-095 and how can I set aLL parameter to defauLt factory. Best regards HossEIN ASKARI POOR ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 11/30/2016 2:04:31 PMNew subject after splitting |
|
11/30/2016 9:31 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello, 6SN1135-1BA12-0DA0 - Simodrive 611 A spindle drive module 30/40 A 6SN1123-1AA00-0DA1 - Simodrive 1 axis power module 80 A User can not replace 611A module by 611D module. The faulty one is analoge & the second one is digital. So they are in-compatible. Another point is you cannot use 611A control card i.e. 6SN1121-0BA11-0AA1 with digital power module. i.e. with 6SN1123-1AA00-0DA1. HTH. |
11/30/2016 5:15 PM | |
Posts: 16 Rating: (0) |
Dear sir First I check this manual for power module and control unit (page 15) and after I replaced power module I attach manual . Please check that Thank you Attachment75802285611A_IA.PDF (904 Downloads) |
11/30/2016 5:30 PM | |
Posts: 1 Rating: (0) |
plc bus fault how can remove |
11/30/2016 5:38 PM | |
Posts: 16 Rating: (0) |
Dear sir Please check this picture. Thank you |
12/1/2016 7:13 AM | |
Joined: 10/17/2007 Last visit: 10/9/2024 Posts: 4039 Rating: (354) |
I think you can try to change P051=4 (Hex), the change P095, after change you must set P052=1 --save to EEPROM, I did not check manual, it is possible --you write down all you parameters, the make you control card new start up, then you can change P095. Go to down load SIMODRIVE 611A Start UP manual for Google or Siemens WEb
|
If you like my comments please |
|
Follow us on