7/3/2009 3:23 PM | |
Joined: 10/7/2005 Last visit: 7/11/2024 Posts: 3009 Rating:
|
Hello sanju757 I gather from your questions that you have NOT used Step5 nor worked with S5 PLC's before. As such I strongly recommend that you have a look at the Step5 manual which has all the info on how to set up a project, go online, download and upload blocks, monitor variables etc. You shoudl have the manual already on your PG and/or on the Step5 CD that you may have. Nonethless,please find below the downlaod link for the manual: STEP 5/ST V7.1 manual Other than that, your PG should have a (grey) cable with it that has a 25 PIN Sub D connector on one end and a 15 PIN Sub D connector on the other. The 25 Pin goes onto your PG720 and the 15 Pin onto your 928B CPU. I hope this helps |
Cheers |
|
7/3/2009 7:32 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating:
|
Hello, When you have Siemens PG you can use 6ES5 734-2BF00 cable. Description of this cable you can find in Connecting cable from PG 7xx to programmable controllers AG 90 U ... AG 155 U . And one tip: PG720 under STEP5 on-line (PC timeout) Hope this will helpful. Best regards, Hristo Mihalev |
This contribution was helpful to
1 thankful Users |
Follow us on