5/9/2016 5:30 PM | |
Joined: 7/22/2010 Last visit: 6/11/2024 Posts: 3 Rating:
|
I need to control pH range between 0 to 14. How can I control an acid pump and caustic pump to control pH in the logo? How can you control two outputs with the PI instruction? I would also need a deadband between the ranges of the pumps so they never run at the same time. Any help would be appreciated. Thank you, Adam ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/10/2016 9:50:03 AMNew subject after splitting |
|
5/11/2016 1:03 AM | |
Joined: 7/22/2010 Last visit: 6/11/2024 Posts: 3 Rating:
|
I have a Logo8. The analog signal coming in is 4-20ma and the 2 analog outputs are 4-20ma. Best Regards, Adam |
Follow us on