8/24/2006 4:36 PM | |
Posts: 2 Rating: (0) |
Hello. I've a lot of data stored into tables : (text files or access database tables) First colomn of eachtable is theacquisition date. Second column of each table is the acquisition hours. All other column are the dataacquiredby a system (other than Siemens and WINCC). I want for each column of data to create a view of trends in my WINCC project. An example of datafile to import is attached to this message . I have WinCC V6 SP4 with connectivity pack and SQL server SP4 installed on my PC. I try with DTS import but I can find the right procedure. Does I create the tags in WinCC project before the import ? Do you have a procedure or documentation with this explain Could you help me to do this, please. I thank you for your help Pierre Attachmentbut_brut_03.zip (501 Downloads) |
8/25/2006 11:17 AM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating: (151)
|
First of all, the Connectivity Pack is used to query data already in the WinCC database. So it is no use in this situation. |
Follow us on