6/24/2009 6:35 PM | |
Joined: 1/4/2008 Last visit: 2/27/2024 Posts: 703 Rating: (96) |
Hello Ayman, the FAQs aren't a part of this forum, but you can send a useful information with asking to create a FAQ and even receive some money for this. Look here: http://support.automation.siemens.com/WW/view/en/11774683 Regards Sydney |
6/25/2009 10:53 AM | |
Joined: 1/4/2008 Last visit: 2/27/2024 Posts: 703 Rating: (96) |
Hello, sorry I haven'tnoticed that it's availableonly in Intranet user view, You can change it on the right side at the bottom (if possible). So if you have some useful things you can post it here in forumas a Tip thread. In addition you can contact the moderators by the PM or you can create an issue about any post. Regards Sydney |
Last edited by: Sydney at: 6/25/2009 10:55 AM |
|
6/25/2009 1:20 PM | |
Joined: 9/1/2005 Last visit: 5/8/2024 Posts: 4100 Rating: (193) |
Dear Ayman Elotaify, Sydney is to fast for me And I agree with him. If you think that you got an idea for a new faq or for updating you could publish it here within the conferences. Then create an issue about the posting and I will mark the thread as idea for new faqs (of course we got a mechanism to do that ) The other way, ifa person (which is not a Siemens employee) has a good idea for a new faq, is to send a email Address: online-support.automation@siemens.com Please wrote "FAQ-issue" or something like that within the subject. Great that you want to share your knowledge with all other users! Best regards CS Moderator |
Last edited by: CS Moderator at: 7/7/2009 10:33 AMMy Forum is the place to personalize your profile, |
|
This contribution was helpful to4 thankful Users |
Follow us on