4/1/2024 9:13 AM | |
Joined: 6/16/2022 Last visit: 6/2/2024 Posts: 1 Rating: (0) |
Hi.. We are using CPU412-5H PN/DP with CP443-1 for MB TCP/IP communication. We are using FB907 (MB REDSV) block for red communication. I could read or write only holding register (40001) address. But I couldn't read or write in input register (30001) address. For communication testing, I am using s71200 CPU and Modscan64 as a client, even I couldn't read or write the input register. How can read or write in input register? Kindly support us to resolve the problem. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/02/2024 08:19:57New subject after splitting |
|
Follow us on