7/13/2017 8:59 AM | |
Joined: 9/30/2016 Last visit: 4/23/2025 Posts: 936 Rating:
|
I have a small system with a PLC, a comfort panel and two drives that are connected. They are currently connected and are running on software programmed in TIA V13. The system has been reprogrammed with new SW blocks using TIA V14 and the network connections have been deleted and redrawn. I have previously experience that - even though the connections was there and working - there was errors indicated in the TIA portal because the connections was in the wrong order or in a slightly different position. How can I see that the connections are "identical" when I look at the old V13 SW and the new V14 SW - see also the attached screenshots ? AttachmentDevices & networks.docx (88 Downloads) |
Follow us on