5/25/2021 12:31 PM | |
Joined: 9/30/2016 Last visit: 8/15/2024 Posts: 914 Rating: (6) |
Please also see the attached screenshots. This project in is WinCC 7.0. I need some lines in different colors that are switched on only when a certain bit is set. I have a (unsigned 16 bits - see pic 68.jpg) status signal available under my Tag Management and I know which bits to use for which line but how do I connect to specific bits in WinCC 7.0 (like I can do it in WinCC 7.4 - see pic 61.jpg). AttachmentEB5 SD A.zip (359 Downloads) |
5/25/2021 3:06 PM | |
Joined: 9/30/2016 Last visit: 8/15/2024 Posts: 914 Rating: (6) |
Hello Georg Berghof, Thank you for answering again. Maybe what you are suggesting could solve my problem - but I am convinced there is a better (more similar to the original) solution. It is a DIFFERENT solution that what is used by our current automation supplier in WinCC 7.4 and WinCC 7.5 projects. I would prefer to make the logic as similar as possible for easier maintenance and trouble shooting. The solution I would prefer is under properties - miscellaneous - display (as shown in pic 61) where you are suggesting I pick an invisible color under properties - line colors - Colors. I know I sent a screeenshot from under animations which was a mistake (even though switching a line on/off COULD have been classified as an animation). I think I found the place for the selection of the tag (is it not the same tagname as I wrote in the notepad window?) but how do I select the actual bit? Can I write the tagname in the field or must I browse all the way to the tagname?
AttachmentEB5 SD B.zip (357 Downloads) |
5/31/2021 9:29 AM | |
Joined: 9/30/2016 Last visit: 8/15/2024 Posts: 914 Rating: (6) |
Does no one really have a answer for this or is it just so obvious that it does not merit an answer? |
5/31/2021 11:08 AM | |
Joined: 10/3/2010 Last visit: 9/27/2024 Posts: 1562 Rating: (191) |
Perhaps attached example might get you started? |
B r g d s , |
|
5/31/2021 2:16 PM | |
Joined: 10/3/2010 Last visit: 9/27/2024 Posts: 1562 Rating: (191) |
What you show in your screenshot, is exactly the same as in V7.0. So I don't understand the problem. |
B r g d s , |
|
6/1/2021 7:56 AM | |
Joined: 9/30/2016 Last visit: 8/15/2024 Posts: 914 Rating: (6) |
Hi again SteBo, Thank you for answering. Hmm - very strange - in MY WinCC 7.0 it looks quite different - and I don't see where I get to pick the bit (as in my OP). Please see the attached screenshots (this time from 7.0) and explain (for dummies) how I can pick the bit.
AttachmentEB5 SD D.zip (347 Downloads) |
Follow us on