7/7/2021 11:31 AM | |
Joined: 9/30/2016 Last visit: 11/11/2024 Posts: 914 Rating: (6) |
I will do my best and some of the information can hopefully be seen on the attached screenshots too: It is a 314 PLC with the following number: 6ES7 314-1AF11-0AB0 firmware 2.0 What is the CP? I was hoping to connect the the PLC with a standard network cable with RJ45 plus in each end as I do with almost all of our machines. I also have a USB cable with "standard" USB plug in one end and mini USB in the other end but I think that is for direct connection to the Siemens drives we have. I THINK there is another cable in my coworkers bag (he is on vacation now) I have borrowed earlier but I am not sure. It might have been to connect to SSD drives. I just tried looking in the Industry Mall but it is still not clear to me - which options are there to connect to the "SIMATIC S7-300, CPU 314 CPU WITH MPI INTERFACE INTEGRATED 24 V DC POWER SUPPLY 64 KBYTE WORKING MEMORY" ? If you tell me which cable / converter(s) I need I will search for them - I am pretty sure we have it somewhere.
AttachmentGK4 connection A.zip (370 Downloads) |
Last edited by: xmnj at: 07/07/2021 11:31:22 |
|
7/7/2021 12:45 PM | |
Joined: 9/30/2016 Last visit: 11/11/2024 Posts: 914 Rating: (6) |
Thanks again ChristophD and Hati, Please look at the screenshots. I have a normal laptop with 3 vm-ware machines each with Simatic Managers but one with WinCC 7.0, one with WinCC 7.4 and one with WinCC 7.5 - so I am running the vm-ware machine that matches the version of WinCC on the HMI server. Does the adapter I found look correct - and did I find the correct settings - I cannot really match 187 in baud rate?
AttachmentGK4 connection B.zip (384 Downloads) |
7/7/2021 1:25 PM | |
Joined: 9/21/2012 Last visit: 11/14/2024 Posts: 4199 Rating: (474) |
Buy the one i linked, it's the latest version of the adapter. |
Follow us on